BACnet settings - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active
Note: BACnet IP routing requires an Ethernet connection. The SBH Wi-Fi Client does not support BACnet IP routing.
To configure the SBH system bus settings, complete the following steps:
  1. Navigate to the Settings tab.
  2. Under the Settings tab, select the BACnet Settings option and adjust the following parameters:
    • Device Object Identifier – Identifies the SBH as a unique device on a BACnet network. Adjustable: 0 to 4194303, default 1.
    • MAC Address – Sets the address on the system bus for the MS/TP network. Adjustable: 4 to 127, default 117.
    • Network Number – Sets the routing address for devices under the SBH. Adjustable: 1 to 65534, default 64999. It is best practice to leave the network number on the default setting.
    • Baud Rate – Sets the baud rate of the System Bus and can be used to match the Baud rate for different controllers connected to the System Bus. Adjustable to 1200, 9600, 19200, 38400 and 76800. All Verasys controllers and Smart Equipment will default to 38400.