Alarm notifications - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
User Guide
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

You can configure email and text alarms using alarm notifications. Click the Alarm Notifications from the Settings tab to set the parameters. First, you must connect the SBH to an Ethernet network and define the DNS servers. See the Ethernet section of this document to set up the Ethernet connection for the SBH. The following table describes each alarm notification parameter. Refer to the following video link https://docs.jci.com/bas/verasys-setup-users-alerts.

Table 1. Alarm notification
Field Setting Description
Enabled Default is Off. Set to On to use the email and text alarm function.
Use TLS Set to Yes to use transport layer security (TLS).
Host SMTP relay host address where alarms are sent.
Port When the server sends an email to the host, this is the port the server uses.
From Email Address This email address appears as the sender of the email.
Site Name In the subject line of the email, the site name appears with the controller it came from, and the alarm. You can specify the name of the site in the subject line.
User Name To connect to the host server you must log in. This is the user name of that login.
Set Password This check box opens up a dialog box to enter the password. You must open the dialog box with the password entered in order to test alarms. When testing is complete, click Save.
Password The password for the account used to log on to the SMTP host.
Test Email Address You can use this dialog box to test an email. Make sure you open the password dialog box and enter a password. Press Send when you have finished writing the email. The top of the screen indicates if the system sent the email successfully.