Administration - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
User Guide
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

The Administration tab is located on the Settings tab. You can configure users and user permissions from the Administration tab. By default, the system creates an Admin user role. For first-time log on information, see Connecting to the SBH and refer to the Verasys Smart Building Hub (SBH) Quick Start Guide SBH300 (Part No. A16381V57K).

After you have logged on, you are prompted to change the default password. This dialog box is where you change the Admin password again, configure the Admin user, or add more users to the system. Configuring multiple users helps distinguish who makes adjustments to the systems and when they access the system. See the following table.

Table 1. New User
Field Description
Name Identifies the individual obtaining an account.
Username Identifies the user. This unique identifier can not contain spaces.
Password/Verify Password The password must contain 12 or more characters, 1 lower case letter, 1 uppercase letter, 1 number and 1 special character.
Roles

Roles include:

Tenant: This role provides access to devices, facility, and schedules. Tenant permissions include device homepage, alarm notifications, and password settings. Refer to Verasys Tenant User Guide LIT-12013613.

Tech: This role is similar to the admin role. Tech permissions provide access to the Settings tab.

  • Facility: Viewable and adjustable

  • Wi-Fi Access Point: Viewable and adjustable

  • Ethernet: Viewable and adjustable

  • Load Shedding: Viewable and adjustable

  • Global Shutdown: Viewable and adjustable

  • Alarm Notification: Viewable, not adjustable

  • Software Updates: Able to install updates

  • System Settings: Viewable and adjustable

Admin: This role provides access to all settings and adjustments within the Verasys System.

Alarm Notification Level Sets the user alarm notification levels. The four options include:

Disable: User does not receive notifications via email or text message.

Service: User receives all alarms (service, service priority, and critical).

Service Priority: User receives only service priority and critical alarms.

Critical Alarms: User only receives critical alarms.

Email address and SMS message notifications You can enter the email address and SMS notifications into the following fields:
  • Email Address 1 field
  • Email Address 2 field