Introduction to Verasys - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

The Verasys system provides bundled equipment and controls solutions that are well-proven. The Verasys system features both simple, configurable controllers and HVACR equipment from the factory or installed in the field. You can use Verasys to configure many HVACR controls applications for one building or an entire enterprise comprised of multiple buildings, without using special programming tools or control engineering.



Verasys has a key role in the Internet of Things (IoT) ecosystem in the light commercial market. The technology is based on the Smart Equipment technology and uses the core assets of Johnson Controls Metasys product lines. You can use Verasys to create installation use cases that provide standard feature sets for the light commercial space.