Configuring a two-condition interlock - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

Procedure

  1. If you want, provide a name and description for your interlock.
  2. On the Interlock Condition area, from the Device dropdown list select the device that you want to associate with the interlock to show all the points you can assign between the device and the interlock.
  3. From the Points dropdown list, select the Point you want to associate with the interlock. This action makes the point part of the interlock logic.
  4. From the Operator dropdown list, select the operator for the point.
  5. Enter the value.
  6. Enter the Differential +/- variance.
  7. Under Input Conditions, select Two Conditions (AND) or Two Conditions (OR).
  8. Follow a similar process to steps 3-5 above for first input condition .
  9. In the Interlock Action section, select the device and point which you want to perform the interlock action. You can configure an action when the interlock is true or flase.
  10. Click Save to enable the interlock.