Interlocks - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
User Guide
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

Through the interlocks feature, the Verasys control system can create and execute simple logical automation functions. The interlocks feature can also interface entitled devices with external devices and equipment through physical connections. For example, you can connect the VAC with the generic IOM application.