Editing graphics on a Verasys device - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

To edit standard graphics on a Verasys device, complete the following steps:

  1. Click Devices.
  2. Select the device that you want to change the graphics on.
  3. To change the graphic, select the Change Graphic button on the devices homepage.
  4. On the Change graphics home page, navigate to Uploaded Images.
  5. Choose an existing image or select the Upload button to upload your own graphic. The graphic must be under 15 megapixels and less than 10 MB.
  6. Click Apply.