Facility - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

Facility is the first screen that appears when you log on to an SBH. The Facility home page displays the devices that are directly serving tenant areas. The Facility feature provides an enhancement to the previous Spaces view and includes HVAC, lighting, and other miscellaneous applications found in light commercial and mid-market buildings . It also provides a summary of the current system status and enables changes to setpoints and modes.

On the Facility view, the devices are categorized into two tabs at the top of the screen:

  • HVAC
  • Lighting

These tabs dynamically populate depending on the type of equipment connected to the SBH. Refer to the following video link https://docs.jci.com/bas/verasys-facility-overview.