Editing device details - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

Complete the following steps on the Devices screen to edit device names and descriptions:

  1. Click Edit Device Details.
  2. Edit the device names and descriptions. Both the name and description have a 30-character limit. If any device name or description is greater than 30 characters, no changes can be saved.
  3. Click Save Device Details.