Devices - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

The Devices tab on the navigation tree provides a list of all the online and offline Verasys devices. The system organizes the devices based on the bus connection type. The system bus address appears in a solid blue box on the left followed by the device name, device description, and status.

To view the devices, complete the following steps:

  1. In the navigation tree, click the Devices tab. The system scans all the devices on the system bus and creates a list of all the online devices.
  2. Click a specific device to explore the parameters. The first selection in all devices is the home screen. The home screen consists of a graphic section and status section. The Status section contains information about current system conditions. Use the additional buttons on the left side of the screen to navigate to the different menus for the device. For more information about the graphics, see the Graphics section in this document.
  3. Click the Devices tab to return to the main Devices screen.