You can use the data share feature to share the value of a point from the list of shareable points from one device to other devices. The data selection defines what object or parameter is available for sharing to controllers with similar objects. The source selection sets which controller is the source. The destination selection sets the controller that receives the data.
Outdoor Air Temperature (OAT) is an example of data share. Instead of installing a physical sensor on every unit, you can connect a single OAT sensor and share the value to all other equipment. Occupied setpoints are another example. Set one device as the source and all other devices as the destination. You can simply change the setpoints on one device and share to all others.
To configure data share, complete the following steps:
- Click the Data Share tab.
- Click the Add Data Share button.
- In the Data drop-down list, select an object or parameter.
- In the Source drop-down list, select the controller that you want to define as the source.
- In the Destination drop-down list, select the controllers that you want to share the data with.
The following table lists the shareable data points.
Controllers | Data in | Data out |
---|---|---|
Smart Equipment Rooftop Unit, SE-SPU100xx-1 | Humidity Setpoint | Humidity Setpoint |
Indoor Air Quality | Indoor Air Quality | |
Occupied Cooling Setpoint | Occupied Cooling Setpoint | |
Occupied Heating Setpoint | Occupied Heating Setpoint | |
Outdoor Air Temperature | Outdoor Air Humidity | |
Standby Cooling Setpoint | Outdoor Air Temperature | |
Standby Heating Setpoint | Standby Cooling Setpoint | |
Unoccupied Cooling Setpoint | Standby Heating Setpoint | |
Unoccupied Heating Setpoint | Unoccupied Cooling Setpoint | |
Zone/Space Temperature | Unoccupied Heating Setpoint | |
Warm/Cool Adjust | ||
Zone/Space Temperature | ||
Discharge Air Temperature | ||
Terminal Equipment Controller, SE-TEC3xxx-0 | Common Setpoint | Common Setpoint |
Humidity Setpoint | Humidity Setpoint | |
Occupied Cooling Setpoint | Occupied Cooling Setpoint | |
Occupied Heating Setpoint | Occupied Heating Setpoint | |
Outdoor Air Temperature | Outdoor Air Temperature | |
Standby Cooling Setpoint | Return Air Humidity | |
Standby Heating Setpoint | Standby Cooling Setpoint | |
Unoccupied Cooling Setpoint | Standby Heating Setpoint | |
Unoccupied Heating Setpoint | Unoccupied Cooling Setpoint | |
Zone/Space Temperature | Unoccupied Heating Setpoint | |
Warm/Cool Adjust | ||
Zone/Space Temperature | ||
Discharge Air Temperature | ||
Verasys Generic IO Controller, LC-VAC1002-0 | NONE | Indoor Air Quality |
Outdoor Air Humidity | ||
Outdoor Air Temperature | ||
Zone/Space Temperature | ||
Discharge Air Temperature | ||
Verasys Constant Volume Application, LC-VAC1000-0, LC-VAC3000-0 | Discharge Air Temperature | Discharge Air Temperature |
Humidity Setpoint | Humidity Setpoint | |
Outdoor Air Temperature | Indoor Air Quality (CO2) | |
Standby Cooling Setpoint | Outdoor Air Humidity | |
Standby Heating Setpoint | Outdoor Air Temperature | |
Unoccupied Cooling Setpoint | Standby Cooling Setpoint | |
Unoccupied Heating Setpoint | Standby Heating Setpoint | |
Zone Temperature Setpoint | Unoccupied Cooling Setpoint | |
Indoor Air Quality (CO2) | Unoccupied Heating Setpoint | |
Zone Humidity | Zone Temperature Setpoint | |
Occupied Cooling Setpoint | Zone/Space Temperature | |
Occupied Heating Setpoint | Zone Humidity | |
Zone Temperature | ||
Third-party RTU controller, LC-VEC100-0 | Outdoor Air Temperature | Outdoor Air Temperature |
Zone Temperature from ZEC | Supply Air Temperature | |
Return Air Temperature | ||
CO2 | ||
VAV Box Controller, LC-ZEC510-x, LC-ZEC310-0 | Occupied Cooling Setpoint | Indoor Air Quality |
Occupied Heating Setpoint | Occupied Cooling Setpoint | |
Standby Cooling Setpoint | Occupied Heating Setpoint | |
Standby Heating Setpoint | Standby Cooling Setpoint | |
Unoccupied Cooling Setpoint | Standby Heating Setpoint | |
Unoccupied Heating Setpoint | Unoccupied Cooling Setpoint | |
Warmer/Cooler Adjust | Unoccupied Heating Setpoint | |
Zone Temperature | Warmer/Cooler Adjust | |
Zone Temperature | ||
Advanced Terminal Unit Controller, LC-ATC1xxx-0 | Fan Mode | Fan Mode |
Heat Cool Mode | Heat Cool Mode | |
Indoor Air Quality | Indoor Air Quality | |
Outdoor Air Temperature | Outdoor Air Temperature | |
Standby Cooling Setpoint | Standby Cooling Setpoint | |
Standby Heating Setpoint | Standby Heating Setpoint | |
Unit Enable | Unit Enable | |
Unoccupied Cooling Setpoint | Unoccupied Cooling Setpoint | |
Unoccupied Heating Setpoint | Unoccupied Heating Setpoint | |
Zone/Space Temperature | Zone/Space Temperature |