When doors remain open during economizer operation, economizer effectiveness is reduced and there are building pressurization problems. To avoid these problems, use power exhaust functions. For systems with ducted returns, use power exhaust fans. The return duct pressure drop causes most barometric relief dampers to function poorly or not at all. The Smart Equipment RTU can control the power exhaust whenever the economizer is operating. If you use a VEC100, building pressure and exhaust fans must be controlled by equipment other than the VEC100 RTU Controller.