Zone Voting Logic - Verasys - LIT-12012331 - General System Information - Verasys System - 4.0

Verasys System Changeover Bypass Zoning System Design Application Note

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012331
Version
4.0
Revision date
2020-03-24
Product status
Discontinued

The COBP Zoning System uses zone voting logic. The Zone Coordinator carries out the following actions:

  • Monitors the status of the individual zone: the zones vote for either heating or cooling based on how the current zone temperature deviates from the current zone temperature setpoint.
  • Processes the votes and determines whether the RTU must provide heating or cooling to the zones.
  • Commands the RTU to the appropriate mode of either heating or cooling.
  • The Zone Coordinator continues to monitor the zones and changes the operating mode of the RTU to accommodate the zones’ needs.