General Zoning Design Overview - Verasys - LIT-12012331 - General System Information - Verasys System - 4.0

Verasys System Changeover Bypass Zoning System Design Application Note

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012331
Version
4.0
Revision date
2020-03-24
Product status
Discontinued

Procedure

To design a COBP Zoning System, complete the following steps:

  1. Determine the number and location of zones.
  2. Size the zone dampers.
  3. Size the central unit.
  4. Plan the duct system design.
  5. Select air diffusers.
  6. Size the bypass dampers.
  7. Locate the static pressure sensor and probe.