Configuring the Internet connection Wi-Fi Client - Verasys - LC-SBH300-0 - LC-SBH300-0C - LC‑SBHPNL-01 - Network gateway - Smart Building Hub

Verasys Smart Building Hub (SBH300) Quick Start Guide

Product name
Smart Building Hub
Document type
Quick Start Guide
Document revision
C
Revision date
2024-03-28
Product status
Active
docpartnumberlabel
Part No.
Part number
A16381V57K

Before you begin

The SBH300 Wi-Fi Client uses the WPA2-PSK protocol. Ensure that the external Wi-Fi router is set to WPA2-PSK mode.

Do not turn Wi-Fi Client and Ethernet on at the same time. When you use the Wi-Fi Client, make sure that Ethernet is off. To turn off Ethernet, navigate to Settings > Ethernet. From the Enabled list, select Off.

About this task

To connect the SBH300 to the Internet over Wi-Fi, complete the following steps:

Procedure

  1. Plug the Wi-Fi adapter into the USB port.
  2. Log on to the SBH300 local UI. See Connecting to the SBH with the Wi-Fi access point.
  3. Click Settings > Wi-Fi Client.
  4. From the Enabled list, select On.
  5. Click the Select SSID button.
  6. From the SSID list, select the SSID of the wireless network you want to connect to.
    Note: Ensure the SSID of the wireless network does not contain special characters, such as ',*,@,$,!,#. Special characters prevent the SBH300 connecting to wireless networks.
  7. In the Passphrase field, enter the passphrase of the wireless network.
  8. Click Save. To see your changes, refresh the page.
    Note: If you do not intend to permanently connect the SBH to the Internet, it is best practice to use the Wi-Fi Client to temporarily connect to the Internet to ensure that the SBH300 downloads the latest firmware packages.