Connecting to the SBH with the Wi-Fi access point - Verasys - LIT-12012324 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Network and IT Guidance Technical Bulletin

Product
Network and Communications > Gateways and Routers > Smart Building Hub
Document number
LIT-12012324
Version
5.1
Revision date
2024-03-11
Product status
Active

About this task

Complete the following steps to access the SBH300 local UI and monitor equipment connected to the SBH300 on the Device List.

Procedure

  1. Plug the Wi-Fi adapter into the USB port.
  2. Verify that the Wi-Fi AP LED is flashing.
  3. Access the Wi-Fi settings on your Wi-Fi connected mobile phone, tablet, or computer.
    Note: Turn off VPN applications, such as Zscaler or Cisco® AnyConnect, on your device.
  4. Select the SBH300's default Wi-Fi access point (AP) SSID and enter the SBH300's default Wi-Fi AP Passphrase, located on the label of the Verasys Smart Building Hub (SBH300) Quick Start Guide (Part No. A16381V57K) included with the SBH300.
  5. Open a web browser and enter https://192.168.142.1 as the browser address.
    Note: Your web browser may display a warning that your connection is not private or secure. This message appears because the security certificate is a privately signed certificate and cannot be verified by the web browser. You can ignore this warning and click Advanced or Show more details, and then click the Proceed to https://192.168.142.1 (unsafe) link.
  6. Use the factory default UI Username and UI Password, located on the label of the Verasys Smart Building Hub (SBH300) Quick Start Guide (Part No. A16381V57K) included with the SBH300.
  7. Read and accept the SBH300 license agreement.
  8. The first time you log on to the SBH300, you must change the admin password, Wi-Fi AP Passphrase, and the Wi-Fi AP SSID.
    Important: After you change the Wi-Fi AP passphrase or Wi-Fi AP SSID, the web server restarts and you need to rejoin the SBH300 Wi-Fi network using the new SSID and passphrase. On some computers and mobile devices, click on the original Wi-Fi AP network before you rejoin the network with the new passphrase.

Results

When you logon to the SBH300 connected to the MS/TP network, all the devices on the network that have unique addresses appear in the device list and are available to configure.