Chain of trust - Verasys - LIT-12012324 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Network and IT Guidance Technical Bulletin

Product
Network and Communications > Gateways and Routers > Smart Building Hub
Document number
LIT-12012324
Version
5.1
Revision date
2024-03-11
Product status
Active

Multiple users can use a chain of trust to create and use software on a system where digital certificates are verified in a chain configuration, and their keys are not stored directly in hardware. When you attempt to use the SBH300 without the software being digitally signed, the UI issues warnings. The signing authority only signs boot programs that enforce security, such as only running programs that are themselves signed, or allowing only signed code to have access to certain features of the machine. This process may continue for several layers, through one or more intermediate certificates. These create a chain of trust from the root certificate, issued by the CA, to the end-entity certificate that enables the final software to run.