USB ports - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

The SBH300 has two USB 2.0 host (type A) ports and one USB 2.0 client (type micro) port. The USB host ports are dedicated for the Wi-fi USB access point.

  • Do not use the USB port as a charging port.
  • Do not connect devices other than those specified in Johnson Controls® technical documentation.
  • Use the USB ports only when needed.
Table 1. USB port pin designations
Pin number for both ends of the cable Signal name
1 +5 VDC
2 Data -
3 Data +
4 No connection
5 Ground