USB adapters - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document type
Installation Guide
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

Connect the Wi-Fi adapter that comes with the SBH300 into either of the USB 2.0 host (type A) ports.

The following table lists the USB Wi-Fi adapters the SBH300 supports.

Table 1. SBH300 USB Wi-Fi adapters
Manufacturer Model name
LM Technologies® LM808
D-Link® DWA-131 E
D-Link DWA-171 A
D-Link DWA-171 C
Netgear® A6100
TP-Link® Archer
Premiertek® PT-8811AU

For more information about ordering a USB Wi-Fi adapter, see Accessories.