System bus communications connections - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

To connect the SBH300 to the system bus for communication, use the System Bus adapter on the SBH.

The SBH300 has a dedicated default system bus address of 116. You can change the default address in the BACnet Settings menu. Ensure that the SBH has a unique address on the system bus network. The system bus can only accommodate one SBH300.

Performance of the SBH300 varies based on the amount of traffic it accommodates.