Ethernet port - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1
Verasys Smart Building Hub (SBH300) Installation Guide
Product
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active
The Ethernet port on the SBH300 is an 8-pin RJ-45 jack. The maximum cable length is 100 m (328 ft).