System bus port - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

You can connect to the SBH300 RS-485 system bus port through a blue, 4-terminal, system bus terminal block plug. You can also temporarily connect the system bus to a device with the 6-pin RJ12 cable. For data transmission and other specifications, see Technical specifications.