Wiring - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document type
Installation Guide
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

The SBH300 supports a maximum capacity of 100 single-zone devices across the System Bus and all Zone Buses.

You can hardwire and wirelessly connect the controllers to the SBH300, as the SBH300 supports both connection types simultaneously. To wirelessly connect the controllers, connect the TMR coordinator to the SBH300 and connect one TMR router to each equipment controller. One TMR coordinator supports up to 35 wireless devices. You can add an additional TMR coordinator to the SBH300 to connect a maximum capacity of 70 wireless devices.
Note: Configure each TMR coordinator with a different PAN ID before you wire them to the SBH300.