Status indication LEDs - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document type
Installation Guide
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active
The SBH300 uses status LEDs to indicate functional states according to the LED map shown in the following table:
Table 1. SBH300 LED designations and operation
LED name Color Status Description
POWER Purple Off The device has no power.
On solid Primary voltage supplies power.
FAULT Red Off The device is operating normally.
On solid Missing hardware or software, operating system is not yet initialized, or reset is in progress.
Slow flashes then fast flashes Reset button is being pressed.
Two flashes per second Start up sequence.
Five flashes per second Other fault.
ETHERNET ACTIVITY Green Off Ethernet cable is not connected.
Flashes Data transmission.
ETH LINK SPEED Yellow Off No network connection.
On solid 100 Mbps
Blue On solid 1 Gbps
RUN Green Off No power or waiting for processes to start.
On solid OS and all monitored processes have started and the device is ready to use.
UPGRADE Green Off No firmware upgrade is in progress.
On solid Firmware upgrade is in progress.
SYSTEM BUS Green Off System Bus is unavailable.
On solid System Bus is available and data is transferring.
Wi-Fi AP Green Off Wi-Fi adapter is not connected.
On solid The Wi-Fi adapter is connected and client is connected.
Flashing Broadcasting SSID and no client is connected.
SYSTEM EOL Yellow Off FC EOL is switched off.
On solid FC EOL is switched on.
Wi-Fi CLIENT Blue Off Wi-Fi Client is off.
Flashing Wi-Fi Client is trying to connect to the network.
On solid Wi-Fi Client is on.
CLOUD n/a n/a Not currently supported.
CELLULAR n/a n/a Not currently supported.