Smart Equipment Controller updates - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document type
Installation Guide
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

You can update the RTU UCB Contollers directly from the SBH interface without the need for a physical USB drive. To update the firmware of your RTU UCB Controllers, ensure you have access to the remote firmware file you want to install. The file name must be in the format x.x.x.x.remoteUpgrade.secusb.pkg or x.x.x.x_SE-xxxxxxx-x_ remote_ota_update.pkg If the second file type has a .zip file extension, it must be changed to .pkg. To update Controllers, complete the following steps:

  1. Log on to the SBH Local UI and navigate to the Settings menu.
  2. Click Software Update > Controller Update
  3. A list of available controllers appears. Click Upload to upload the remote firmware file.
  4. Click the empty checkboxes for the controllers you want to update.
  5. Click the Install button to begin the update process.
  6. After the installation is complete the updated firmware version is displayed in the Current Firmware column.
Note: Do not interrupt the installation process as it occurs. Ensure that you have a stable network connection and do not log off of the SBH Local UI until the update is complete.
Note: The Smart Equipment Controller must be at version 4.3.1.24 or later to use the OTA update feature.