Reset to factory defaults - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

About this task

The Reset to Factory Defaults function resets all device settings including user profiles. The function also resets your SSL certificate to the Johnson Controls self-signed certificate that is included in the device. This function is for administrators who want to clear all user profiles from a device. The Reset to Factory Defaults function does not change the version of the software. If you run a software upgrade, the SBH300 retains the upgraded software version and does not reset to the factory default version.

To reset to factory defaults, complete the following steps:

Procedure

  1. Press and hold the RESET button for six seconds. After two seconds, the FAULT LED flickers slowly. After an additional four seconds of holding the RESET button, the FAULT LED changes to a faster flicker.
  2. Release the RESET button within three seconds of seeing a fast flicker. The FAULT LED continues to flicker quickly.
  3. Within five seconds, press the RESET button again, and then immediately release it to confirm that you want to reset to factory defaults. If you do not press the RESET button to confirm within five seconds, the reset operation is canceled.

Results

The Fault LED may flicker for up to eight minutes before all the LEDs turn on during reboot and start-up. All device settings reset to factory defaults. The LEDs stop flashing for two seconds, and then the LEDs return to normal operation based on the current state of the device.

Important: To access the SBH300 after a reset to factory defaults, you must use the default log on credentials, see Factory default log on credentials. You can also find the default credentials on the Smart Building Hub (SBH300) Quick Start Guide (Part No. A16381V57K) included with the SBH300 and on the label on the back of the SBH300.