Reset button operation and descriptions - Verasys - LIT-12014293 - LC-SBH300-0 - LC-SBH300-0C - LC-SBH300-0LA - LC-SBHPNL-01 - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document type
Installation Guide
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

Use the following reset functions on the SBH300 if you lose your password or if you want to restore the unit to factory defaults:

  • Network Reset
  • Reset to Factory Defaults

Use the instructions in the following sections according to the type of reset you require. For both resets, the following information applies:

  • The reset button is located through a small hole on the front of the device. To reach the reset button, use a small screwdriver or similar tool.
  • If the SBH300 is connected to the network when you press the reset button, it disconnects from the network.
  • If you press and hold the reset button for more than nine seconds, the reset operation cancels.
  • If a fault condition already exists, the reset button does not work.