Network reset - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

About this task

The Network Reset function resets Wi-Fi access point settings. Use this function if you forget your Wi-Fi connection information. To reset the Wi-Fi access point settings, complete the following steps:

Procedure

  1. Press and hold the RESET button for two seconds. The FAULT LED flickers slowly.
  2. Release the RESET button within three seconds. The FAULT LED continues to flicker slowly.
  3. Within five seconds, press the RESET button again, and then immediately release it to proceed with the reset. If you do not press the RESET button to confirm within five seconds, the reset operation is canceled.

Results

The Wi-Fi access point SSID and passphrase are set to factory defaults. The LEDs stop flickering for two seconds, then the LEDs return to normal operation based on the current state of the device.