Wall mounting - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document type
Installation Guide
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active

Procedure

  1. Pull the bottom two mounting clips downward to their extended positions.
  2. Mark mounting hole locations on the wall. Use the dimensions shown in Figure 1, or hold the bracket against the wall and mark the hole locations through the mounting clips.
    Note: The screw holes on the SBH300 can accommodate M4 and #8 screws.
  3. Drill holes in the wall based on the locations marked in step 2. Insert wall anchors for each hole if necessary.
  4. Hold the device in place, insert the screws through the mounting clips and into the screw holes, and then carefully tighten all screws.
    Important: Do not overtighten the mounting screws. Overtightening the screws can damage the mounting clips or bracket.
    Figure 1. Front and side view mounting dimensions, mm (in.)