Location considerations - Verasys - LIT-12014293 - LC-SBH300-0 - LC-SBH300-0C - LC-SBH300-0LA - LC-SBHPNL-01 - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document type
Installation Guide
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active
Follow these guidelines when you mount the SBH300:
  • Mount the SBH300 in areas free of corrosive vapors and observe the environmental limitations listed in the Technical specifications section.
  • Solid objects including walls, duct work, cabinets, doors, and glass can impede the Wi-Fi signal. Minimize the number of barriers between the connected computer or mobile device and the SBH300. Use line of sight, if possible.
  • Metal objects such as cabinet doors, enclosures, and pipes, and concrete objects such as pillars, walls, and ceilings can limit Wi-Fi service.
  • Do not mount the SBH300 outside.