LED test sequence at start-up - Verasys - LIT-12014293 - LC-SBH300-0C - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Network gateway - SBH300 Smart Building Hub - 5.1

Verasys Smart Building Hub (SBH300) Installation Guide

Product
Document type
Installation Guide
Document number
LIT-12014293
Version
5.1
Revision date
2024-03-11
Product status
Active
During start-up, the SBH300 automatically initiates a self test to verify correct operation. When you connect the supply power, the following LED lighting sequence occurs:
  • The POWER LED turns purple.
  • The FAULT LED is on solid for approximately 45 seconds and then flashes for approximately 2 minutes and 30 seconds. The FAULT LED then turns off and the RUN LED turns solid when the SBH300 is fully functional.