Field Bus Communications Connections - Verasys - LC-MAP1860-1SL - Supervisory controller - Verasys Smart Building Hub

Verasys Smart Building Hub (SBH) Installation Guide LC-MAP1860-1SL

Product
Building Automation Systems > Building Automation Systems > Verasys Smart Building Hub
Document revision
A
Revision date
2021-03-26
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10737-00180

To connect the Smart Building Hub to the FC field bus for communication, connect the RJ-12 cable to the Smart Building Hub and wire the other end to the FC bus using the field adapter connector.

Note: The Smart Building Hub has a dedicated MS/TP bus address of 03. The number of Smart Building Hub units that can be connected simultaneously to one MS/TP bus depends on the number of FC ports available and connected to the bus. The MS/TP bus can accommodate one Smart Building Hub on the FC bus.
Note: Performance of the Smart Building Hub varies based on the amount of traffic.