The following table contains the settings for the available groups of trends.
Name (Reference name) |
Buffer size |
Sample interval |
Availability condition |
---|---|---|---|
Trend : Inputs : Binary Input x (x = 1 to 4) | |||
Binary Input x | 25 | At every change of value (0) | Details : Inputs : Binary Input x : Present = Present |
Trend : Inputs : Analog Input x (x = 5 to 9) | |||
Analog Input x | 96 |
User Configurable Default : 900 s |
Details : Inputs : Analog Input x : Trend = Enable |
Trend : Outputs : Binary Output x (x = 1 to 6) | |||
Binary Output x | 25 | At every change of value (0) | Details : Outputs : Binary Output x : Present = Present |
Trend : Outputs : Analog Output x (x = 1 to 3) | |||
Analog Output x | 96 |
User Configurable Default : 900 s |
Details : Outputs : Analog Output x : Trend = Enable |
Trend : Netsensor x : Zone Temperature (x = 199 to 206) | |||
Zone Temperature | 96 |
User Configurable Default : 900 s |
Details : Netsensor Plug and Play : Netsensor x : Trend = Enable |
Trend : Netsensor x : Zone Humidity (x = 199 to 206) | |||
Zone Humidity | 96 |
User Configurable Default : 900 s |
Details : Netsensor Plug and Play : Netsensor x : Trend = Enable |
Trend : Netsensor x : Indoor Air Quality (x = 199 to 206) | |||
Zone CO2 | 96 |
User Configurable Default : 900 s |
Details : Netsensor Plug and Play : Netsensor x : Trend = Enable |