Introduction - Verasys - LIT-12013364 - LC-VAC1000-0 - Smart equipment controller - Verasys Lighting Controller - 4.2

Verasys Sideloop Controller Application Note

Product
Controls > Lighting Controls > Verasys Lighting Controller
Document number
LIT-12013364
Revision date
2021-07-16
Product status
Discontinued

The Verasys® sideloop controller application is part of the Verasys application library.

To download the application, log in to verasyscontrols.com and access the application library in the Product Information & Support > Device Updates section. Download the application package file and install it on the Verasys Application Controller (VAC), LC-VAC1000-0. See Updating the VAC for more information.

This document describes the application, wiring, and characteristics of the controller. The parameters for this controller are adjustable in the field, but the application is fixed.

If you have further questions about the application, contact Verasys support.