To set the VAC address using the SBH, perform the following steps:
Procedure
In the SBH, navigate to the VAC controller.
Navigate to the Controller > Network menu of the VAC controller.
Note: The default address is 4. If another controller uses this address,
disconnect the other address 4 controller from the trunk temporarily while
you configure the controller, or use the procedure in Setting the VAC address using the local display.
Click the Up and Down arrows to
select the address, or enter the address directly.