You can use the Verasys Sideloop application to design simple loops that control various types of equipment. System configuration involves the following activities:
- Define inputs, outputs, and netsensors
- Enable the number and type of control loops that you want
- Configure each control loop
You can define the following types of control loops:
- Analog control loop
- Binary control loop
- Multistage control (MSC) loop
The following table lists the maximum number of control loops that you can enable, and the available control strategies for the system logic.
| Control loop type | Maximum number of loops | Available control strategies |
|---|---|---|
| Analog | 3 |
Note: You can also define an additional binary interlock for this
control loop type.
|
| Multistage | 1 |
Note: You can also define an additional binary interlock for this
control loop type.
|
| Binary | 6 |
|