The Input/Output Module (IOM) is a simple point multiplexer that provides monitoring of up to two analog inputs, two binary inputs, and scheduling of up to four binary outputs.
The IOM uses either the System Manager (SM) or Verasys Smart Building Hub (SBH) to monitor and control auxiliary points in a facility. Monitor input points using the SM and schedule binary output points with the SM scheduling feature.
Refer to the Commercial Comfort System (CCS) Product Bulletin (LIT-12011347) or the Verasys System Product Bulletin (LIT-12012342) for important product application information.
Figure 1. Input/Output Module