Wiring - Verasys - Bulb controller - Verasys Equipment Controller

Verasys Equipment Controller (VEC) Installation Guide

Product
Controls > Application Controls > Verasys Equipment Controller
Document revision
C
Revision date
2020-02-24
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10143-1272

Observe the following guidelines when wiring a field controller:

WARNING
  • Risk of Electric Shock
  • Disconnect power from the controller before making any adjustments. Do not touch any part of the printed circuit board while power is applied. Failure to follow these precautions can result in personal injury or death.
Avertissement
  • Risque de décharge électrique
  • Déconnecter l'alimentation du controller avant toute opération de réglage. Veiller à ne toucher aucune partie du circuit imprimé lorsque celui-ci est sous tension. Le non-respect de ces précautions peut provoquer des blessures graves, voire mortelles.
WARNING
  • Risk of Electric Shock
  • Disconnect or isolate all power supplies before making electrical connections. More than one disconnection or isolation may be required to completely de-energize equipment. Contact with components carrying hazardous voltage can cause electric shock and may result in severe personal injury or death.
Avertissement
  • Risque de décharge électrique
  • Débrancher ou isoler toute alimentation avant de réaliser un branchement électrique. Plusieurs isolations et débranchements sont peut-être nécessaires pour -couper entièrement l'alimentation de l'équipement. Tout contact avec des composants conducteurs de tensions dangereuses risque d'entraîner une décharge électrique et de provoquer des blessures graves, voire mortelles.
Important:
  • Do not exceed the controller electrical ratings. Exceeding controller electrical ratings can result in permanent damage to the controller and void any warranty.
  • Use copper conductors with a rating of at least 75°C (167°F). Make all wiring in accordance with local, national, and regional regulations.
  • Electrostatic discharge can damage controller components. Use proper electrostatic discharge precautions during installation, setup, and servicing to avoid damaging the controller.

For the wiring diagram, refer to the application note or quick start guide document for the VEC application you use.

For detailed information on configuring and wiring an MS/TP Bus, zone bus (system bus), and sensor bus (SA bus), refer to the Verasys BACnet MS/TP Communications Technical Bulletin (LIT-12012362).