Input and Output Terminal Blocks - Verasys - Bulb controller - Verasys Equipment Controller

Verasys Equipment Controller (VEC) Installation Guide

Product
Controls > Application Controls > Verasys Equipment Controller
Document revision
C
Revision date
2020-02-24
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10143-1272

On most field controller models, all of the input terminal blocks or spade terminals are mounted on the bottom of the controller and the output terminal blocks and spade terminals are mounted on the top of the controller. A package of terminals (PK-KIT1810-0) will come with the controller so if you wish to convert to terminal blocks you have that option. See Table 1 for more information about I/O terminal functions, requirements, and ratings.