Field Wiring - Verasys - Bulb controller - Verasys Equipment Controller

Verasys Equipment Controller (VEC) Installation Guide

Product
Controls > Application Controls > Verasys Equipment Controller
Document revision
C
Revision date
2020-02-24
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10143-1272

For all I/O terminals listed in Table 1, use the appropriate gauge wiring. For all the spade terminals used in this application, follow the guidelines in Table 1 and use a screw terminal.

Note: Use WECO 130 Series or WIELAND® Electric 8105B. A maximum rated torque of 4.5 lb·in is acceptable when you use the WECO 130 Series terminal blocks.