Use the local display or Smart Building Hub (SBH) to set up device addresses. Before operating field controllers on a bus, you must set a valid and unique device address for each controller on the bus.
On the zone bus, device addresses 4 through 127 are the valid addresses for VECs.
Refer to the Verasys BACnet MS/TP Communications Technical Bulletin (LIT-12012362) for more information on field controller device addresses and how to set them on MS/TP buses.
| Device Address | Use on Description |
|---|---|
| 0 | Reserved for Zone Bus Supervisory Controller (not for use on field controllers). |
| 1 to 3 | Reserved for peripheral devices (not for use on field controllers). |
| 4 to 127 | Used for MS/TP master devices (field controllers) that are hard-wired to a sensor bus or zone bus. |