Application - Verasys - Bulb controller - Verasys Equipment Controller

Verasys Equipment Controller (VEC) Installation Guide

Product
Controls > Application Controls > Verasys Equipment Controller
Document revision
C
Revision date
2020-02-24
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10143-1272

The Verasys® Equipment Controller (VEC) is part of the SMART Equipment® Controller family. The VECs run pre-engineered applications and provide the inputs and outputs required to monitor and control HVAC equipment.

The VECs operate on an RS-485 BACnet® MS/TP Bus as BACnet Advanced Application Controllers (B-AACs) and integrate into Johnson Controls® and third-party BACnet systems.

The VECs include an integral real-time clock that enables the controllers to monitor and control schedules, calendars, trends; and the integral real-time clock can operate for extended periods of time as a stand-alone controllers when offline from the system network.

Important: Use this Verasys Equipment Controller only as an operating control. Where failure or malfunction of the VEC controller could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the Verasys Equipment Controller.
Important : Utiliser ce Verasys Equipment Controller uniquement en tant que dispositif de contrôle de fonctionnement. Lorsqu'une défaillance ou un dysfonctionnement du controller risque de provoquer des blessures ou d'endommager l'équipement contrôlé ou un autre équipement, la conception du système de contrôle doit intégrer des dispositifs de protection supplémentaires. Veiller dans ce cas à intégrer de façon permanente d'autres dispositifs, tels que des systèmes de supervision ou d'alarme, ou des dispositifs de sécurité ou de limitation, ayant une fonction d'avertissement ou de protection en cas de défaillance ou de dysfonctionnement du Verasys Equipment Controller.