Okta authorization and API access - Verasys - LIT-12013026 - LC-ENT100-01 - LC-SBH300-0 - LC-SBH300-0LA - LC-SBHPNL-01 - Building automation software - Verasys Enterprise - 5.0

Verasys Enterprise Security and IT Guide

Product
Building Automation Systems > Building Automation Systems > Verasys Enterprise
Document type
User Guide
Document number
LIT-12013026
Version
5.0
Revision date
2023-09-19
Product status
Active

Verasys Enterprise uses Okta to authorize user access.

Okta requests access tokens from a security token service and then use the tokens to communicate with APIs. This practice reduces complexity on the client application and the API, because authentication and authorization are centralized. The Okta specification defines several authorization grants that can be used to coordinate authentication of a user and grant access to resources that the user owns.