Configuring roles and rights - Verasys - LIT-12013026 - LC-ENT100-01 - LC-SBHPNL-01 - LC-SBH300-0 - LC-SBH300-0LA - Building automation software - Verasys Enterprise - 5.0

Verasys Enterprise Security and IT Guide

Product
Building Automation Systems > Building Automation Systems > Verasys Enterprise
Document number
LIT-12013026
Version
5.0
Revision date
2023-09-19
Product status
Discontinued

About this task

Create roles and configure permissions for roles to customize user access to Verasys Enterprise. For example, create an administrator role and a user role. Configure the administrator role with read and write privileges, and the user role with read privileges.

Procedure

To create a role, complete the following steps:

  1. In the nine-dot menu, click Setup.
  2. On the Setup page, click Users.
  3. In the Role tab, in the Role field, enter a name for the role that you want to create and click Add to create the new role. You can also enter a description in the Description field.
    The new role appears in the table of roles at the bottom of the page.

What to do next

To assign permissions to roles, complete the following steps:

  1. In the nine-dot menu, click Setup.
  2. On the Setup page, click Users.
  3. In the Access Rights tab, select a role from the Select Role drop-down list.
  4. Use the View and Edit checkboxes in the table at the bottom of the screen to enable or disable access to specific portions of the Verasys Enterprise system.
  5. Click Save to save the permissions.