Verasys parameters and objects - Verasys - LIT-12013067 - LC-IOM3711-0 - LC-VAC1000-0 - LC-VAC3000-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27
Table 1. Parameters and objects
Men Object or parameter Description Adjustable Defaults Range
Alarm: Critical Low Temperature Alarm This alarm occurs when the low temperature alarm binary input is triggered. If either heating or cooling output is proportional, the unit shuts down if triggered. If the unit does not have proportional outputs and has an economizer, the system commands the economizer to close and the unit runs. Read only    
Emergency Shutdown Alarm This alarm occurs if someone triggers the emergency shutdown object under the status menu. Read only    
Zone High Temperature Alarm If the zone temperature exceeds the cooling setpoint by 5°F this alarm occurs. Read only    
Zone Low Temperature Alarm If the zone temperature drops below the heating setpoint by 5°F this alarm occurs. Read only    
Supply Fan Fault If you add a supply fan status sensor and the commanded value of the fan does not match the binary input for fan status, this alarm occurs. Read only    
Unit in Purge Mode If either the emergency mode or binary input triggers a purge, this alarm occurs and the unit opens the dampers to 100 percent. Read only    
Alarm: Service Priority Heating Ineffective Alarm This alarm occurs if the heat cool diagnostics are set to True and you have a supply air temperature sensor. If you request heating and the temperature does not rise by an expected amount of a defined period of time, an alarm occurs. Read only    
Cooling Ineffective Alarm This alarm occurs if the heat cool diagnostics are set to True and you have a supply air temperature sensor. If you request cooling and the temperature does not fall by an expected amount of a defined period of time, an alarm occurs. Read only    
Zone Temperature Sensor Failure This alarm occurs if a zone temperature sensor is connected and receives a reliable input that is suddenly disconnected.
Note: If the sensor was connected by mistake, you can trigger the relearn system input from the Details menu on the Sensors section.
Read only    
Return Air Temperature Sensor Failure This alarm occurs if a return air temperature sensor is connected and receives a reliable input that is suddenly disconnected.
Note: If the sensor was connected by mistake, you can trigger the relearn system input from the Details menu on the Sensors section.
Read only    
Supply Air Temperature Sensor Failure This alarm occurs if a supply air temperature sensor is connected and receives a reliable input that is suddenly disconnected.
Note: If the sensor was connected by mistake, you can trigger the relearn system input from the Details menu on the Sensors section.
Read only    
Outside Air Temperature Sensor Failure This alarm occurs if an outside air temperature sensor is connected and receives a reliable input that input is suddenly disconnected.
Note: If the sensor was connected by mistake, you can trigger the relearn system input from the Details menu on the Sensors section.
Read only    
Alarm: Service Priority (continued) Mixed Air Temperature Sensor Failure This alarm occurs if a mixed air temperature sensor is connected and receives a reliable input that is suddenly disconnected.
Note: If the sensor was connected by mistake, you can trigger the relearn system input from the Details menu on the Sensors section.
Read only    
Air Temperature Sensor Fault This alarm occurs if the economizer fault detection is enabled and the mixed air or outside air temperature sensor becomes unreliable. Read only    
Damper Modulation Fault This alarm occurs if the economizer fault detection is enabled and the difference between the Economizer Damper % Command and the Economizer Damper Position is greater than the Damper Position Error, this fault occurs. Read only    
Econ Excessive Outside Air This alarm occurs if the Economizer fault detection is Enabled and the Economizer Damper Position (feedback) is higher than the Minimum Position by more than the Damper Min Pos Fault Tolerance.This check is performed when the mixed air damper is at its minimum position or is fully closed. Read only    
Econ Operational Fault This alarm occurs if the economizer fault detection is enabled and Economizer Damper Position (feedback) is higher than the minimum position plus the Damper Min Position Fault Tolerance. This check is performed when the mixed air damper is at its minimum position. Read only    
Econ Not Operational Fault This alarm occurs if the economizer fault detection is enabled and Economizer Damper Position (feedback) is less than the minimum position plus the Damper Min Position Fault Tolerance. This check is performed when the economizer is in control. Read only    
Alarm: Service Dirty Filter This alarm occurs when the binary input for the filter status is triggered Read only    
Fan Runtime Alarm This alarm occurs when the runtime of the fan exceeds the runtime limit Read only    
Service Alarm This alarm occurs when the binary input for the service alarm is triggered Read only    
Status Unit Status The current status or state of the unit Read only    
Unit Enable Disables the unit if set to shutdown Adjustable Shutdown  
Emergency Mode Use to manually control the unit to pressurize, depressurize, purge, or shut down.
Note: Generally this point is used in conjunction with an economizer to try to control smoke.
Adjustable Normal  
System Mode Use to control the various states of the unit. Adjustable Auto  
Occupancy Override Use to override any occupied control condition. If this is set to anything besides Not Set, the unit remains in the mode you selected until you return this object to Not Set. Adjustable Not Set  
Occupied Status Displays the current occupancy mode of the unit Read only    
Zone Temperature Present value of the zone temperature NS sensor Read only    
Return Air Temperature AI Present value of the return air temperature Read only    
Supply Air Temperature AI Present value of the supply air temperature analog input Read only    
Mixed Air Temperature AI Present value of the mixed air temperature analog input Read only    
Zone Humidity Present value of the zone humidity NS sensor Read only    
Zone Humidity AI Present value of the zone humidity analog input Read only    
Zone Quality Present value of the zone air quality NS sensor Read only    
Return CO2 Sensor AI Present value of the return CO2 sensor analog input Read only    
Operational Outdoor Air Temperature Present value of the outdoor air temperature analog input Read only    
Economizer Status The current status of the economizer Read only    
Fan Status The current status of the fan Read only    
Cooling Status The current state of the cooling Read only    
Heating Status The current state of heating Read only    
Humidification The current state of humidification Read only    
Dehumidification The current state of dehumidification Read only    
Hot Gas Reheat Status The current state of the hot gas reheat Read only    
Summary: HVAC Zone Zone Temperature Present value of the zone temperature NS sensor Read only    
Return Air Temperature AI Present value of the return air temperature Read only    
Temperature Setpoint The occupied temperature setpoint that the unit is trying to achieve Adjustable 72°F 61°F to 85°F
Setpoint Adjust The adjustment that the zone temperature NS sensor adds or subtracts from the temperature setpoint Read only    
Zone Humidity Present value of the zone humidity NS sensor Read only    
Zone Humidity AI Present value of the zone humidity analog input Read only    
Zone Quality Present value of the zone air quality NS sensor Read only    
Return CO2 Sensor AI Present value of the return CO2 sensor input Read only    
Summary: Fan Supply Fan BO Present value of the supply fan binary output Read only    
Fan Status BI Present value of the supply fan status binary input Read only    
Supply Fan Speed AO Present value of the Supply fan speed analog output Read only    
Summary: Cooling Effective Cooling Setpoint The temperature setpoint the cooling tries to achieve. This setpoint is calculated with the occupancy state, load shed command, temperature setpoints, setpoint adjustments, and deadband. Read only    
Cooling Status The current state of the cooling Read only    
Cooling % Command The current percent command for cooling Read only    
Cooling Stage 1 BO Present value of cooling stage 1 output Read only    
Compressor Stage 1 Accumulated Runtime The accumulated runtime of stage 1 Read only    
Cooling Stage 2 BO Present value of cooling stage 2 output Read only    
Compressor Stage 2 Accumulated Runtime The accumulated runtime of stage 2 Read only    
Cooling Stage 3 BO Present value of cooling stage 3 output Read only    
Compressor Stage 3 Accumulated Runtime The accumulated runtime of stage 3 Read only    
Cooling Stage 4 BO Present value of cooling stage 4 output Read only    
Compressor Stage 4 Accumulated Runtime The accumulated runtime of stage 4 Read only    
Summary: Heating Effective Heating Setpoint The temperature setpoint the heating tries to achieve. This setpoint is calculated with the occupancy state, load shed command, temperature setpoints, setpoint adjustments, and deadband. Read only    
Heating Control Status The current state of the heating Read only    
Heating % Command The current percent command for heating Read only    
Heating Stage 1 BO Present value of heating stage 1 output Read only    
Heating Stage 1 Accumulated Runtime The accumulated runtime of stage 1 Read only    
Heating Stage 2 BO Present value of heating stage 2 output Read only    
Heating Stage 2 Accumulated Runtime The accumulated runtime of stage 2 Read only    
Heating Stage 3 BO Present value of heating stage 3 output Read only    
Heating Stage 3 Accumulated Runtime The accumulated runtime of stage 3 Read only    
Heating Stage 4 BO Present value of heating stage 4 output Read only    
Heating Stage 4 Accumulated Runtime The accumulated runtime of stage 4 Read only    
Summary: Heat Pump Effective Cooling Setpoint The temperature setpoint the cooling tries to achieve This setpoint is calculated with the occupancy state, load shed command, temperature setpoints, setpoint adjustments, and deadband. Read only    
Effective Heating Setpoint The temperature setpoint the heating tries to achieve. This setpoint is calculated with the occupancy state, load shed command, temperature setpoints, setpoint adjustments, and deadband. Read only    
Heat Pump % Command The current percent command for heat pump Read only    
Compressor Stage 1 BO The present valve of compressor stage 1 Read only    
Compressor Stage 2 BO The present valve of compressor stage 2 Read only    
Reversing Valve BO The present valve of the reversing valve Read only    
Cooling Status The current state of the cooling Read only    
Heating Status The current state of the heating Read only    
Summary: Supplemental Heating Supp Heating Stage 1 BO The present valve of supplemental heating stage 1 Read only    
Supp Heating Stage 2 BO The present valve of supplemental heating stage 2 Read only    
Summary: OA Damper Minimum OA Damper AO The present valve of outside air damper analog output Read only    
Minimum OA Percent The minimum outside air damper percent setpoint Adjustable 10% 0% to 100%
Summary: Economizer Economizer Status The current state of the economizer Read only    
Mixed Air Damper Position AI The present value of the mixed air damper feedback analog input Read only    
Mixed Air Damper AO The present value of the mixed air damper analog output Read only    
Minimum OA Percent The minimum outside air damper percent setpoint Adjustable 10% 0% to 100%
Economizer Switchover Setpoint The setpoint at which the economizer switches to use the damper for free cooling Adjustable 68°F 40°F to 80°F
Operational Outdoor Air Temperature The present value of the outside air temperature analog input Read only    
Mixed Air Temperature AI The present value of the mixed air temperature analog input Read only    
Supply Air Temperature AI The present value of the supply air temperature analog input Read only    
Low Limit Temp Setpoint The setpoint at which the damper starts to modulate closed if the mixed air sensor senses a temperature that is colder than this setpoint Adjustable 45°F -50°F to 250°F
Supply Air Low Limit Setpoint The setpoint at which the damper starts to modulate closed if the supply air sensor senses a temperature that is colder than this setpoint Adjustable 55°F -50°F to 250°F
Zone Quality The present value of the zone air quality sensor Read only    
Return CO2 Sensor AI The present value of the return air quality analog input Read only    
CO2 Reset A The low setpoint for the demand ventilation control. This is the setpoint at which the damper minimum position starts to increase. Adjustable 800 ppm 0 to 2000 ppm
CO2 Reset B The high setpoint for the demand ventilation control. This is the setpoint at which the damper minimum position meets the maximum position. Adjustable 1000 ppm 0 to 2000 ppm
Summary: Humidifier Humidity Setpoint The setpoint that the humidifier controls to Adjustable 40% 0% to 100%
Humidifier BO The present value of the humidifier enable binary output Read only    
Humidification AO The present value of the humidifier analog output Read only    
Humidification The current status of the humidifier Read only    
Zone Humidity The present value of the zone humidity sensor Read only    
Zone Humidity AI The present value of the zone humidity analog input Read only    
Summary: Dehumidification Dehumidification Setpoint The setpoint that the unit dehumidifies to. Adjustable 60% 0% to 100%
Dehumidification The current status of the dehumidification control Read only    
Hot Gas Reheat Status The current status of the hot gas bypass. Read only    
Zone Humidity The present value of the zone humidity sensor Read only    
Zone Humidity AI The present value of the zone humidity analog input Read only    
Hot Gas Bypass Valve BO The present value of the hot gas bypass valve binary output Read only    
Summary: Diagnostic Econ Fault Active The present value of the economizer fault. Forms part of the economizer fault detection diagnostics (FDD) alarms Read only    
Air Temperature Sensor Fault The present value of the air temperature sensor fault. Forms part of the economizer FDD alarms Read only    
Econ Operational Fault The present value of the economizer operational fault. Forms part of the economizer FDD alarms. Read only    
Econ Not Operational Fault The present value of the economizer not operational fault. Forms part of the economizer FDD alarms. Read only    
Economizer Excessive Outside Air The present value of the economizer excessive outside air fault. Forms part of the economizer FDD alarms Read only    
Damper Modulation Fault The present value of the economizer damper failure to modulate fault. Forms part of the economizer FDD alarms Read only    
Fan Runtime The present value of the fan runtime Read only    
Fan Runtime Alarm The present value of the fan runtime alarm Read only    
Cooling Ineffective Alarm The present value of the cooling ineffective alarm. Part of the heat cool alarms based on supply air temperature Read only    
Heating Ineffective Alarm The present value of the heating ineffective alarm. Part of the heat cool alarms based on supply air temperature Read only    
Summary: Load Shed Load Shed Active The present value of the load shed command Read only    
Load Shed Adjust The limit that the setpoints separate when a load shed adjustment command occurs Adjustable 4°F 0°F to 5°F
Load Shed Rate Limit The rate that the setpoints separate at when a load shed adjustment command occurs Adjustable 0.066°F / Min 0°F to 1°F / Min
Commissioning: Commission Outputs Start Commissioning To start the commissioning process set this to trigger, then command the outputs below. Adjustable Normal Normal / Trigger
Supply Fan When you set Start Commissioning to trigger this object, it tests the supply fan. Adjustable Off Off / On
Fan Speed Command When you set Start Commissioning to trigger this object, it tests the supply fan output. Adjustable 0% 0% to 100%
Cooling Command When you set Start Commissioning to trigger this object, it tests the cooling command output. Adjustable 0% 0% to 100%
Cool Stage 1 When you set Start Commissioning to trigger this object, it tests the cooling stage 1 output. Adjustable Off Off / On
Cool Stage 2 When you set Start Commissioning to trigger this object, it tests the cooling stage 2 output. Adjustable Off Off / On
Cool Stage 3 When you set Start Commissioning to trigger this object, it tests the cooling stage 3 output. Adjustable Off Off / On

Cool Stage 4

When you set Start Commissioning to trigger this object, it tests the cooling stage 4 output.

Adjustable

Off

Off / On

Compressor 1 When you set Start Commissioning to trigger this object, it tests the compressor 1 output. Adjustable Off Off / On
Compressor 2 When you set Start Commissioning to trigger this object, it tests the compressor 2 output. Adjustable Off Off / On
Reversing Valve When you set Start Commissioning to trigger this object, it tests the reversing valve output. Adjustable Off Off / On
Heating Command When you set Start Commissioning to trigger this object, it tests the heating command output. Adjustable 0% 0% to 100%
Heat Stage 1 When you set Start Commissioning to trigger this object, it tests the heating stage 1 output. Adjustable Off Off / On
Heat Stage 2 When you set Start Commissioning to trigger this object, it tests the heating stage 2 output. Adjustable Off Off / On
Heat Stage 3 When you set Start Commissioning to trigger this object, it tests the heating stage 3 output. Adjustable Off Off / On
Heat Stage 4 When you set Start Commissioning to trigger this object, it tests the heating stage 4 output. Adjustable Off Off / On
Supplemental Heat Stage 1 When you set Start Commissioning to trigger this object, it tests the supplemental heat stage 1 output. Adjustable Off Off / On
Supplemental Heat Stage 2 When you set Start Commissioning to trigger this object, it tests the supplemental heat stage 2 output. Adjustable Off Off / On
Commissioning: Commission Outputs (continued) Hot Gas Bypass Valve When you set Start Commissioning to trigger this object, it tests the hot gas bypass valve output. Adjustable Off Off / On
Damper Command When you set Start Commissioning to trigger this object, it tests the damper command output. Adjustable 0% 0% to 100%
Humidifier When you set Start Commissioning to trigger this object, it tests the humidifier output. Adjustable Off Off / On
Humidifier Command When you set Start Commissioning to trigger this object, it tests the humidifier command output. Adjustable 0% 0% to 100%
Commissioning: Setpoints Zone Temperature The present value of the zone temperature Read only    
Return Air Temperature AI The present value of the return air temperature analog input Read only    
Temperature Setpoint The zone temperature setpoint when the unit is in the occupied mode. You can raise and lower the control point with this object. Adjustable 72°F 60°F to 85°F
Deadband The deadband is used to separate the effective heating and cooling setpoints so that the unit does not try to control heating and cooling at the same time. For example, setting the temperature setpoint to 72 with a deadband of 2 means the effective cooling is 74 and the effective heating is 70 when the unit is occupied and the setpoint adjust is set to 0. Adjustable 2°F 1-7 delta °F
Setpoint Adjust This is the adjustment value set at the NS sensor. The effective cooling and heating setpoints shift by this amount when the unit is in the occupied mode. Read only    
Effective Cooling Setpoint The temperature setpoint the cooling tries to achieve. This setpoint is calculated with occupancy state, load shed command, temperature setpoints, setpoint adjustments, and deadband. Read only    
Unocc Cooling Setpoint This is the setup setpoint when the unit is in the unoccupied mode. When the zone temperature rises above this value during unoccupied mode the unit cycles on to reduce the temperature. Adjustable 82°F 60°F to 85°F
Standby Cooling Setpoint The system uses the standby cooling setpoint when the occupied status input is set to sense motion and it does not sense motion. Adjustable 77°F 60°F to 85°F
Effective Heating Setpoint The temperature setpoint the heating tries to achieve. This setpoint is calculated with occupancy state, load shed command, temperature setpoints, setpoint adjustments, and deadband. Read only    
Commissioning: Setpoints (continued) Unocc: Heating Setpoint This is the setback setpoint when the unit is placed in unoccupied mode. When the zone temperature drops below this value during unoccupied mode, the unit cycles on to reduce the temperature. Adjustable 61°F 60°F to 85°F
Standby Heating Setpoint The system uses the standby heating setpoint when the occupied status input is set to sense motion and it does not sense motion. Adjustable 66°F 60°F to 85°F
Temp Occupancy Time If a person presses the NS sensor temporary occupancy button, this is how long the unit is set to the occupied mode. Adjusting to 0 disables this feature. Adjustable 60 Minutes 0 to 120 Minutes
Commissioning: Fan Fan Only Speed The speed of the fan when the system is satisfied Adjustable 50% 0% to 100%
Min Fan Speed The minimum speed the fan starts at when heating and cooling starts and is proportional Adjustable 20% 0% to 100%
Max Fan Speed The maximum speed the fan modulates to when heating and cooling starts and is proportional Adjustable 100% 0% to 100%
Clg Stage 1 Speed When you have staged cooling and activate 1 stage, the system indexes to this speed. Adjustable 70% 0% to 100%
Clg Stage 2 Speed When you have staged cooling and activate 2 stage, the system indexes to this speed. Adjustable 80% 0% to 100%
Clg Stage 3 Speed When you have staged cooling and activate 3 stage, the system indexes to this speed. Adjustable 90% 0% to 100%
Clg Stage 4 Speed When you have staged cooling and activate 4 stage, the system indexes to this speed. Adjustable 100% 0% to 100%
Htg Stage 1 Speed When you have staged heating and activate 1 stage, the system indexes to this speed. Adjustable 70% 0% to 100%
Htg Stage 2 Speed When you have staged heating and activate 2 stage, the system indexes to this speed. Adjustable 80% 0% to 100%
Htg Stage 3 Speed When you have staged heating and activate 3 stage, the system indexes to this speed. Adjustable 90% 0% to 100%
Htg Stage 4 Speed When you have staged heating and activate 4 stage, the system indexes to this speed. Adjustable 100% 0% to 100%
Commissioning: Cooling OAT Cooling Lockout Enabled Enables the outdoor cooling lockout sequence Adjustable Disable Disable / Enable
OA Cooling Lockout Setpoint Setpoint at which outside cooling lockout occurs Adjustable 60°F -50°F to 250°F
Supply Air Setpoint Cooling Min Sets how low the supply air temperature is allowed to reach Adjustable 50°F -50°F to 250°F
Cooling Min On Time Sets the minimum on time for the cooling stages Adjustable 30 Sec 30 to 1800 Sec
Cooling Min Off Time Sets the minimum off time for the cooling stages Adjustable 30 Sec 30 to 1800 Sec
Interstage On Delay Sets the delay between turning on the cooling stages after a stage has been energized Adjustable 30 Sec 30 to 900 Sec
Interstage Off Delay Sets the delay turning off the cooling stages after a stage has been energized Adjustable 30 Sec 30 to 900 Sec
Rotate Enable Sets the ability to rotate the stages based on runtime Adjustable Disable Disable/ Enable
Rotate Cooling Stage Sets the ability to rotate the cooling stages manually Adjustable Normal Normal / Trigger
Failsoft Cooling Value If the cooling is proportional, this is the position the cooling output adjusts to when there is a low limit alarm. Adjustable 100% 0% to 100%
Commissioning: Heating OAT Heating Lockout Enabled Enables the outdoor heating lockout sequence Adjustable Disable Disable / Enable
OA Heating Lockout Setpoint Setpoint at which outside heating lockout occurs Adjustable 69°F -50°F to 250°F
Supply Air Setpoint Heating Max Sets how low the supply air temperature is allowed to reach Adjustable 130°F -50°F to 250°F
Heating Min On Time Sets the minimum on time for the heating stages Adjustable 30 Sec 30 to 1800 Sec
Heating Min Off Time Sets the minimum off time for the heating stages Adjustable 30 Sec 30 to 1800 Sec
Interstage On Delay Sets the delay between turning on the heating stages after a stage has been energized Adjustable 30 Sec 30 to 900 Sec
Interstage Off Delay Sets the delay turning off the heating stages after a stage has been energized Adjustable 30 Sec 30 to 900 Sec
Rotate Enable Sets the ability to rotate the stages based on runtime Adjustable Disable Disable / Enable
Rotate Heating Stage Enables rotate the heating stages manually Adjustable Normal Normal / Trigger
Failsoft Heating Value If the heating is proportional this is the position the heating output adjusts to when there is low limit alarm. Adjustable 100% 0% to 100%
Commissioning: Heat Pump Low OA Lockout Setpoint Setpoint at which the compressors are locked out when the outside air gets too low. Adjustable 48°F -50°F to 250°F
Reversing Valve Polarity Sets whether the output is on for cooling or on for heating. Normally Cool is on for cooling. Normally Heat is on for heating. Adjustable Normally Cool Normally Heat/ Normally Cool
OA Heating Lockout Setpoint Setpoint at which outside heating lockout occurs Adjustable 69°F -50°F to 250°F
Compressor Min On Time Sets the minimum on time for the compressors Adjustable 60 Sec 30 to1800 Sec
Compressor Min Off Time Sets the minimum off time for the compressors Adjustable 60 Sec 30 to1800 Sec
OAT Cooling Lockout Enabled Enables the outdoor cooling lockout sequence Adjustable Disable Disable / Enable
OA Cooling Lockout Setpoint Setpoint at which outside cooling lockout occurs Adjustable 60°F -50°F to 250°F
OAT Heating Lockout Enabled Enables the outdoor heating lockout sequence Adjustable Disable Disable / Enable
Commissioning: Supplemental Heating Supp Min On Time Sets the minimum on time for the supplemental heat stages Read only    
Supp Min Off Time Sets the minimum off time for the supplemental heat stages Read only    
Commissioning: OA Damper Minimum OA Percent Sets the minimum outside air damper position Adjustable 10% 0% to 100%
Commissioning: Economizer Minimum OA Percent Sets the minimum outside air damper position Adjustable 10% 0% to 100%
Economizer Switchover Setpoint Setpoint at which the economizer switches to control for cooling Adjustable 68°F 40°F to 0°F
Low Limit Temp Setpoint Setpoint at which the damper starts to modulate closed if the mixed air sensor senses a temperature that is colder than this setpoint Adjustable 45°F -50°F to 250°F
Supply Air Low Limit Setpoint Setpoint at which the damper starts to modulate closed if the supply air sensor senses a temperature that is colder than this setpoint Adjustable 55°F -50°F to 250°F
CO2 Reset A Low setpoint for the demand ventilation control. This is the setpoint at which the damper minimum position starts to increase. Adjustable 800 ppm 0 to 2000 ppm
CO2 Reset B High setpoint for the demand ventilation control. This is the setpoint at which the damper minimum position reaches the maximum position. Adjustable 1000 ppm 0 to 2000 ppm
Min Pos High Setpoint The minimum position high setpoint for demand ventilation control. Adjustable 90% 0% to 100%
Commissioning: Humidifier Humidity Setpoint Sets the humidity setpoint that the humidifier control to Adjustabl 40% 0% to 100%
Commissioning: Dehumidification Dehumidification Setpoint Sets the humidity setpoint that the dehumidification sequence controls to. Adjustable 60% 0% to 100%
Commissioning: Diagnostic Fan Runtime Limit Sets the runtime limit at which the fan alarm triggers on Adjustable 10000 Hrs 0 to 20000 Hrs
Fan Runtime This parameter displays the current runtime hours of the fan Read only    
Fan Runtime Reset This parameter resets the runtime of the fan Adjustable Normal  
SF Alarm Delay If a supply fan status binary is defined and connected this sets the delay of the supply fan mismatch alarm. Adjustable 60 Sec 60 to 1200 Sec
Heat Cool Alarm Differential Sets how much the supply air temperature must rise or fall for heating or cooling to initiate Adjustable 2°F 0°F to 5°F
Zone Temperature Alarm Delay Sets the zone temperature alarm delay. Note: See Zone Alarm Offset for details on the alarm. Adjustable 900 300 to 1200 Sec
Heat Cool Alarm Delay Sets the amount of time that must pass before the alarm occurs Adjustable 5 minutes 5 to 60 minutes
Zone Alarm Offset Sets how far from the heating or cooling setpoints the zone temperature can reach before an alarm occurs. The zone alarm offset prevents startup from triggering the alarm. Adjustable 5°F 3°F to 8°F
Damper Pos Error Sets the amount of error between the mixed air damper command and the mixed air damper feedback before an alarm occurs Adjustable 8% 0% to 100%
Damper Min Pos Fault Tolerance Sets the amount of error the mixed air damper feedback can have compared to the minimum position Adjustable 5% 0% to 100%
Econ Fault Delay Sets delays for the above alarms so that the moving damper does not trigger False alarms Adjustable 10 Minutes 5 to 60 Minutes
Commissioning: Load Shed Load Shed Adjust The limit that the setpoints separate when a load shed adjustment command occurs Adjustable 4°F 0°F to 5°F
Load Shed Rate Limit The rate that the setpoints separate when a load shed adjustment command occurs Adjustable 0.066°F /Min 0°F to 1°F /Min
Commissioning: PID: Tuning Reset PID Tuning Reset Resets the tuning to defaults for all PIDs that use autotuning Adjustable Off Off / Reset
Commissioning: PID: Economizer: Econ Temp PID Data PID Tuning Type Enables you to tune manually Adjustable Automatic Automatic / Manual
Proportional Band If the PID Tuning Type is set to manual, this sets the proportional band for the loop. Adjustable 16 -100 to 100
Disable Integral Time If the PID Tuning Type is set to manual, you can turn this PID loop into a proportional only loop. Adjustable Enable Disable / Enable
Integral Time If the PID Tuning Type is set to manual, this sets the integral time for the loop. Adjustable 729 Sec

Min 2 times Interval (60)

Max 30 times Interval (60)

Saturation Time If the PID Tuning Type is set to manual, this sets the saturation time for the loop.

You can use the saturation timer to set timing from one state to another. For example, if you switch from heat to cool, the heating loop reaches 0% and the saturation timer must finish before the switch to cooling occurs.

Adjustable 600 Sec

Min > = Interval (60)

Max 3600

Econ T Eff Proportional Band Shows the proportional band the PID loop is using Read only    
Econ T Eff Integral Time Shows the integral time the PID loop is using Read only    
Commissioning: PID: Economizer: Econ Low Temp PID Data PID Tuning Type Enables you to tune manually Adjustable Automatic Automatic / Manual
Proportional Band If the PID Tuning Type is set to manual, this sets the proportional band for the loop. Adjustable 16 -100 to 100
Disable Integral Time If the PID Tuning Type is set to manual, you can turn this PID loop into a proportional only loop.

Adjustable

Enable Disable / Enable
Integral Time If the PID Tuning Type is set to manual, this sets the integral time for the loop. Adjustable 729 Sec

Min 2 times Interval (60)

Max 30 times Interval (60)

Saturation Time If the PID Tuning Type is set to manual, this sets the saturation time for the loop.

You can use the saturation timer to set timing from one state to another. For example, if you switch from heat to cool, the heating loop reaches 0% and the saturation timer must finish before the switch to cooling occurs.

Adjustable 600 Sec

Min > = Interval (60)

Max 3600

Econ LT Eff Proportional Band Shows the proportional band the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Econ LT Eff Integral Time Shows the integral time the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Commissioning: PID: Cooling PID Tuning Type You can tune manually with this parameter. Adjustable Automatic Automatic / Manual
Proportional Band If the PID Tuning Type is set to manual, this sets the proportional band for the loop. Adjustable 16 -100 to 100
Disable Integral Time If the PID Tuning Type is set to manual, you can change this PID loop into a proportional only loop with this parameter. Adjustable Enable Disable / Enable
Integral Time If the PID Tuning Type is set to manual, this sets the integral time for the loop. Adjustable 729 Sec

Min 2 times Interval (60)

Max 30 times Interval (60)

Saturation Time

If the PID Tuning Type is set to manual, this sets the saturation time for the loop.

You can use the saturation timer to set timing from one state to another. For example, if you switch from heat to cool, the heating loop reaches 0% and the saturation timer must finish before the switch to cooling occurs.

Adjustable 600 Sec

Min > = Interval (60)

Max 3600

Clg Eff Proportional Band Shows the proportional band the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Clg Eff Integral Time Shows the integral time the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
HP Eff Proportional Band Shows the proportional band the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
HP Eff Proportional Band Shows the integral time the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Commissioning: PID: Heating PID Tuning Type You can tune manually with this parameter. Adjustable Automatic Automatic / Manual
Proportional Band If the PID Tuning Type is set to manual, this sets the proportional band for the loop. Adjustable 16 -100 to 100
Disable Integral Time If the PID Tuning Type is set to manual, you can turn this PID loop into a proportional only loop. Adjustable Enable Disable / Enable
Integral Time If the PID Tuning Type is set to manual, this sets the integral time for the loop. Adjustable 729 Sec

Min 2 times Interval (60)

Max 30 times Interval (60)

Saturation Time

If the PID Tuning Type is set to manual, this sets the saturation time for the loop.

You can use the saturation timer to set timing from one state to another. For example, if you switch from heat to cool, the heating loop reaches 0% and the saturation timer must finish before the switch to cooling occurs.

Adjustable 600 Sec

Min > = Interval (60)

Max 3600

Htg Eff Proportional Band Shows the proportional band the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Htg Eff Integral Time Shows the integral time the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Htg LT Eff Proportional Band Shows the proportional band the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Htg LT Eff Integral Time Shows the integral time the PID loop is using. The value only updates when the PID loop is running for that process at the time. Read only    
HP Eff Proportional Band Shows the integral time the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
HP Eff Integral Time Shows the integral time the PID loop is using. The value only updates when the PID loop is running for that process at the time. Read only    
Commissioning: PID: Economizer: Supplemental Heating PID Data PID Tuning Type Enables you to tune manually Adjustable Automatic Automatic / Manual
Proportional Band If the PID Tuning Type is set to manual, this sets the proportional band for the loop. Adjustable 16 -100 to 100
Disable Integral Time If the PID Tuning Type is set to manual, you can turn this PID loop into a proportional only loop. Adjustable Enable Disable / Enable
Integral Time If the PID Tuning Type is set to manual, this sets the integral time for the loop. Adjustable 729 Sec

Min 2 times Interval (60)

Max 30 times Interval (60)

Saturation Time

If the PID Tuning Type is set to manual, this sets the saturation time for the loop.

You can use the saturation timer to set timing from one state to another. For example, if you switch from heat to cool, the heating loop reaches 0% and the saturation timer must finish before the switch to cooling occurs.

Adjustable 600 Sec

Min > = Interval (60)

Max 3600

SHtg Eff Proportional Band Shows the proportional band the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
SHtg Eff Integral Time Shows the integral time the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Commissioning: PID: Humidifier PID Tuning Type You can tune manually with this parameter. Adjustable Automatic Automatic / Manual
Proportional Band If the PID Tuning Type is set to manual, this sets the proportional band for the loop. Adjustable 16 -100 to 100
Disable Integral Time If the PID Tuning Type is set to manual, you can change this PID loop into a proportional only loop. Adjustable Enable Disable / Enable
Integral Time If the PID Tuning Type is set to manual, this sets the integral time for the loop. Adjustable 729 Sec

Min 2 times Interval (60)

Max 30 times Interval (60)

Saturation Time

If the PID Tuning Type is set to manual, this sets the saturation time for the loop.

You can use the saturation timer to set timing from one state to another. For example, if you switch from heat to cool, the heating loop reaches 0% and the saturation timer must finish before the switch to cooling occurs.

Adjustable 600 Sec

Min > = Interval (60)

Max 3600

Hum Eff Proportional Band Shows the proportional band the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Hum Eff Integral Time Shows the integral time the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Commissioning: PID: Dehumidification PID Tuning Type You can tune manually with this parameter. Adjustable Automatic Automatic / Manual
Proportional Band If the PID Tuning Type is set to manual, this sets the proportional band for the loop.

Adjustable

16 -100 to 100
Disable Integral Time If the PID Tuning Type is set to manual, you can turn this PID loop into a proportional only loop Adjustable Enable Disable / Enable
Integral Time If the PID Tuning Type is set to manual, this sets the integral time for the loop. Adjustable 729 Sec

Min 2 times Interval (60)

Max 0 times Interval (60)

Saturation Time If the PID Tuning Type is set to manual, this sets the saturation time for the loop.

You can use the saturation timer to set timing from one state to another. For example, if you switch from heat to cool, the heating loop reaches 0% and the saturation timer must finish before the switch to cooling occurs.

Adjustable 600 Sec

Min > = Interval (60)

Max 3600

Dehum Eff Proportional Band Shows the proportional band the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
Dehum Eff Integral Time Shows the integral time the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
HP Dehum Eff Proportional Band Shows the proportional band the PID loop is using. The value updates when the PID loop is running for that process at the time. Read only    
HP Dehum Eff Integral Time Shows the integral time the PID loop is using. The value only updates when the PID loop is running for that process at the time. Read only    
Commissioning: Network Device Name Sets the name of the controller Adjustable   30 characters
Address Sets the address of the controller Adjustable   4 to 127
Controller: Firmware Firmware Main Version Indicates what firmware is in the controller Read only    
Appl SW Version Indicates the software version of the software in the controller Read only    
Application name The name of the application loaded in the controller Read only    
Equipment Template Version The equipment template version Read only    
Equipment Archive Version The equipment archive version Read only    
Equipment View Version The equipment view version Read only    
Controller: Time Time The time the controller is using Read only    
Date The date the controller is using Read only    
Time Zone The time zone the controller is using Adjustable    
Controller: Network Communication Status The status of the controller communication Read only    
Device name Sets the name of the device Adjustable   30 characters
Description Sets the description of the device Adjustable   30 characters
Address Sets the address of the device Adjustable   4 to 127
Operating Baud Rate Shows the operating baud rate of the controller Read only    
Baud Rate Sets the baud rate of the device Adjustable   Auto / 1200 / 9600 /19200 / 38400 / 76800
Bacnet Encoding Type Sets the encoding type the device is using Adjustable  

ISO 1646

(UCS-2) /

ANSI X3.4

(US-ASCII) /

Microsoft DBCS

code page 932

(Japanese Shift JIS) /ISO 10646 (UTF-8)

FC Comm Mode Shows what communication mode the device is using Read only    
Device OID Sets the BACnet ID of the device Adjustable   1-4, 194, 303
Controller: Misc Language Sets the language the controller uses Adjustable   English / French / Spanish
Units Sets the units the controller uses Adjustable   Imperial / Metric
Display Contrast Sets the display contrast for the display on the controller Adjustable   2 to 6
Relearn System Relearns the sensors connected to the controller Adjustable False False / True
Controller: System Configuration Supply Fan Type Set the fan to constant volume or a fixed variable strategy Adjustable Constant Volume Constant Volume Fan / Fixed Variable Fan
Fan Cycling Cycles off the fan if satisfied Adjustable No No / Yes
Cooling Device Type Sets the type of cooling the device uses Adjustable None None / Proportional / Staged / Heat Pump
Number of Cooling Stages Installed Sets the number of stages that the device is set to if the cooling device type is set to staged. Adjustable 0 0 to 4
Number of Heat Pump Stages Installed If the cooling device type is set to heat pump, this sets the number of stages Adjustable 0 0 to 2
Reversing Valve Polarity If the cooling device type is set to heat pump, this sets the reversing valve polarity. Adjustable Normal Normally Heat / Normally Cool
Heating Device Type Sets the type of heating used on the unit Adjustable None  
Number of Heating Stages Installed If the heating device type is set to staged, this sets the number of stages. Adjustable 0 0 to 4
Number of Supp Heating Stages Installed If the heating device type is set to heat pump with supplemental heating, this sets the number of supplemental heat stages. Adjustable 1 0 to 2
Hot Gas Bypass Enable If the system has staged cooling and dehumidification is enabled, this enables a hot gas reheat valve to be energized when dehumidifying. Adjustable Disable Disable / Enable
Economizer Damper Type Defines an economizer or a minimum outside air damper. Adjustable None None / Economizer
Min OA Control Sensor When an economizer is present the system requires a supply air temperature or mixed air temperature to limit the economizer control. This selects which one controls the low limit.
Note: If you select proportional heating or cooling, the mixed air temperature must be present.
Adjustable MA-T MA-T / SA-T
Economizer Fault Detection Enables the economizer fault detection diagnostic sequences. Adjustable Disable Disable / Enable
Humidity Enable Enables the humidity control sequences. Adjustable Disable Disable / Enable
Dehum Enable Enables the dehumidification control sequences. Adjustable Disable Disable / Enable
Heat Cool Diagnostics Enables the heat cool alarms. The heat cool alarms use a supply air sensor to determine if the heating or cooling is working correctly. Adjustable Disable Disable / Enable
Load Shed Allowed If the load shed feature has sent a global load shed command, this feature, you can stop the device from implementing the load shed. Adjustable No No / Yes
Details: Sensors Supply Fan Status Installed If set to yes, the controller generates an alarm when the fan does not match the command value. Adjustable No Yes / No
SAT Sensor Type Sets the resistive curve that the controller uses for the supply air temperature sensor. Adjustable Nickel Nickel / Platinum /A99B / 2.25K NTC / 10K NTC / 10K NTC Type 3
SAT Sensor Offset Sets the offset for the sensor and can calibrate the sensor if it is reading incorrectly. Adjustable 0 - 5°F to +5°F
MAT Sensor Type Sets the resistive curve that the controller uses for the mixed air temperature sensor. Adjustable Nickel Nickel / Platinum/ A99B / 2.25K NTC / 10K NTC / 10K NTC Type 3
MAT Sensor Offset Sets the offset for the sensor and can calibrate the sensor if it is reading incorrectly. Adjustable 0 - 5°F to +5°F
OAT Sensor Type Sets the resistive curve that the controller uses for the outside air temperature sensor. Adjustable Nickel Nickel / Platinum/ A99B / 2.25K NTC / 10K NTC / 10K NTC Type 3
OAT Sensor Offset Sets the offset for the sensor and can calibrate the sensor if it is reading slightly off. Adjustable 0 - 5°F to +5°F
RAT Sensor Type Sets the resistive curve that the controller uses for the return air temperature sensor. Adjustable Nickel Nickel / Platinum/ A99B / 2.25K NTC / 10K NTC / 10K NTC Type 3
RAT Sensor Offset Sets the offset for the sensor and can calibrate the sensor if it is reading slightly off. Adjustable 0 - 5°F to +5°F
Warm/Cool Adjust Range Sets the setpoint adjustability of the NS sensors. Adjustable 3 0 to 5 delta °F
Humidity Sensor Installed Shows if there is an installed sensor and its type. Adjustable Not Installed Not Installed / SAB Sensor / Wired AI Sensor / SAB & Wired Sensor
CO2 Sensor Installed Shows if there is CO2 sensor installed sensor and its type. Adjustable Not Installed Not Installed / SAB Sensor / Wired AI Sensor / SAB & Wired Sensor
Return CO2 Sensor Offset If the hardwired return air CO2 sensor is installed, you can offset it. Adjustable 0 -250 to 250 ppm
Details: Sensors (continued) Occupancy BI Enabled You can use the occupancy binary input to reset the temperature setpoints if motion is not sensed. Adjustable No No / Yes
Relearn System Relearns the sensors connected to the controller. Adjustable False False / True
Details: Inputs Supply Fan Status BI The status of the supply fan status binary input. Read only    
Purge BI The status of the purge command binary input. Read only    
Filter Status BI The status of the filter status binary input. Read only    
Service Alarm The status of the service alarm binary input. Read only    
Low Temperature Limit Fault BI The status of the low temperature limit binary input. Read only    
Outdoor Air Temperature Sensor AI The present value of the outdoor air temperature analog input. Read only    
Mixed Air Damper Position AI The present value of the mixed air damper position analog input. Read only    
Supply Air Temperature AI The present value of the supply air temperature analog input. Read only    
Mixed Air Temperature AI The present value of the mixed air temperature analog input. Read only    
Return Air Temperature AI The present value of the return air temperature analog input. Read only    
Zone Temperature The present value of the zone temperature NS Sensor. Read only    
Zone Humidity The present value of the zone humidity NS Sensor. Read only    
Zone Humidity AI The present value of the zone humidity analog input. Read only    
Zone Quality The present value of the zone quality NS Sensor. Read only    
Return CO2 Sensor AI The present value of the return air quality analog input. Read only    
Zone Occupancy The status of the zone occupancy of the NS Sensor. Read only    
Occupancy Sensor BI The status of the occupancy sensor binary input. Read only    
Setpoint Adjust The present value of the setpoint adjustment of the NS Sensor. Read only    
Details: Outputs: Fan Supply Fan BO The present value of the supply fan binary output. Read only    
Supply Fan Speed AO The present value of the supply fan speed analog output. Read only    
AO Min Out Value Sets the minimum output voltage for the fan speed. Adjustable 0 V 0 V to 10 V
AO Max Out Value This parameter sets the maximum output voltage for the fan speed. Adjustable 10 V 0 V to 10 V
Details: Outputs: OA Damper Minimum OA Damper AO The present value of the outdoor air damper analog output. Read only    
AO Min Out Value Sets the minimum output voltage for the outdoor air damper. Adjustable 0 V 0 V to 10 V
AO Max Out Value Sets the maximum output voltage for the outdoor air damper. Adjustable 10 V 0 V to 10 V
Details: Outputs: Economizer Damper Mixed Air Damper AO The present value of the mixed air damper analog output. Read only    
AO Min Out Value Sets the minimum output voltage for the mixed air damper. Adjustable 0 V 0 V to 10 V
AO Max Out Value Sets the maximum output voltage for the mixed air damper. Adjustable 10 V 0 V to 10 V
Details: Outputs: Cooling Cooling % Command The present value of the cooling command analog output. Read only    
AO Min Out Value Sets the minimum output voltage for the cooling command. Adjustable 0 V 0 V to 10 V
AO Max Out Value Sets the maximum output voltage for the cooling command. Adjustable 10 V 0 V to 10 V
Cooling Stage 1 BO The present value of the cooling stage 1 binary output. Read only    
Cooling Stage 2 BO The present value of the cooling stage 2 binary output. Read only    
Cooling Stage 3 BO The present value of the cooling stage 3 binary output. Read only    
Cooling Stage 4 BO The present value of the cooling stage 4 binary output. Read only    
Hot Gas Bypass Valve BO The present value of the hot gas bypass valve binary output. Read only    
Details: Outputs: Heating Heating % Command The present value of the cooling command analog output. Read only    
AO Min Out Value Sets the minimum output voltage for the cooling command. Adjustable 0 V 0 V to 10 V
AO Max Out Value Sets the maximum output voltage for the cooling command. Adjustable 10 V 0 V to 10 V
Heating Stage 1 BO The present value of the cooling stage 1 binary output. Read only    
Heating Stage 2 BO The present value of the cooling stage 2 binary output. Read only    
Heating Stage 3 BO The present value of the cooling stage 3 binary output. Read only    
Heating Stage 4 BO The present value of the cooling stage 4 binary output. Read only    
Details: Outputs: Heat Pump Compressor Stage 1 BO The present value of the compressor stage 1 binary output. Read only    
Compressor Stage 2 BO The present value of the compressor stage 2 binary output. Read only    
Reversing Valve BO The present value of the reversing valve binary output. Read only    
Hot Gas Bypass Valve BO The present value of the hot gas bypass valve binary output. Read only    
Supp Heating Stage 1 BO The present value of the supp heating stage 1 binary output. Read only    
Supp Heating Stage 2 BO The present value of the supp heating stage 2 binary output. Read only    
Details: Outputs: Humidifier Humidifier BO The present value of the humidifier enable binary output. Read only    
Humidification AO The present value of the humidification analog output. Read only    
AO Min Out Value Sets the minimum output voltage for the humidifier output. Adjustable 0 V 0 V to 10 V
AO Max Out Value Sets the maximum output voltage for the humidifier output. Adjustable 10 V 0 V to 10 V
Set Schedule Occupancy Schedule The internal occupancy schedule for the unit. Adjustable    
Trends Supply Air Temperature AI 96 trend samples at 15 minute increments. Read only    
Mixed Air Temperature AI 96 trend samples at 15 minute increments. Read only    
Outdoor Air Temperature Sensor AI 96 trend samples at 15 minute increments. Read only    
Return Air Temperature AI 96 trend samples at 15 minute increments. Read only    
Zone Temperature 96 trend samples at 15 minute increments. Read only    
Zone Humidity AI 96 trend samples at 15 minute increments. Read only    
Zone Return Humidity 96 trend samples at 15 minute increments. Read only    
Zone Quality 96 trend samples at 15 minute increments. Read only    
Return CO2 Sensor AI 96 trend samples at 15 minute increments. Read only    
Mixed Air Damper Position AI 96 trend samples at 15 minute increments. Read only    
Effective Cooling Setpoint 96 trend samples at 15 minute increments. Read only    
Effective Heating Setpoint 96 trend samples at 15 minute increments. Read only    
Supply Fan BO 20 Samples recorded for each change in value. Read only    
Supply Fan Status 20 Samples recorded for each change in value. Read only    
Unit Status 20 Samples recorded for each change in value. Read only    
Occupancy Status 20 Samples recorded for each change in value. Read only    
Min OA Damper AO 96 trend samples at 15 minute increments. Read only    
Economizer Damper AO 96 trend samples at 15 minute increments. Read only    
Cooling % Command 96 trend samples at 15 minute increments. Read only    
Cooling Stage 1 BO 20 Samples recorded for each change in value. Read only    
Cooling Stage 2 BO 20 Samples recorded for each change in value. Read only    
Cooling Stage 3 BO 20 Samples recorded for each change in value. Read only    
Cooling Stage 4 BO 20 Samples recorded for each change in value. Read only    
Heating % Command 96 trend samples at 15 minute increments. Read only    
Heating Stage 1 BO 20 Samples recorded for each change in value. Read only    
Heating Stage 2 BO 20 Samples recorded for each change in value. Read only    
Trends (continued) Heating Stage 3 BO 20 Samples recorded for each change in value. Read only    
Heating Stage 4 BO 20 Samples recorded for each change in value. Read only    
Compressor Stage 1 BO 20 Samples recorded for each change in value. Read only    
Compressor Stage 1 BO 20 Samples recorded for each change in value. Read only    
Reversing Valve BO 20 Samples recorded for each change in value. Read only    
Supp Heating Stage 1 BO 20 Samples recorded for each change in value. Read only    
Supp Heating Stage 2 BO 20 Samples recorded for each change in value. Read only    
Hot Gas Bypass Valve BO 20 Samples recorded for each change in value. Read only    
Humidification AO 96 trend samples at 15 minute increments. Read only    
Humidifier BO 20 Samples recorded for each change in value. Read only