Tuning - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27

Use the following list to understand the tuning parameters you can select:

  • Proportional Band refers to the change in zone temperature results in a full range change in the equipment outputs. The smaller the Proportional Band, the more aggressively the proportional integral derivative (PID) responds.
  • Integral Time is the amount of time it takes until the integral term of the PID matches the proportional term when the PID has a constant error.
  • Saturation Time is the amount of time the PID loop is at its limit, either 0% or 100%, before saturating low or high. For example, in order to transition from economizer control to economizer + mechanical cooling, the PID for economizer must first saturate high, which is 100% output for Saturation Time.

From the PID Data section of the Commissioning menu, you can set the proportional and integral parameters for each of the control loops. If you select On Off Control, the heating or cooling controller cycles on and off based on a fixed differential from a set point. If PID Tuning Type is set to Manual, the Proportional Band, Integral Time, and Saturation Time are adjustable for each loop. If switched to auto tune, the PID loop starts with the default manual values and then automatically tunes them. For each loop you can see the effective proportional band and integral time. Saturation Time is manually adjustable.