Supply fan control - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27

Use the Fan Cycling parameter in the Details > System Configuration menu to cycle the fan for heating and cooling. If it is set to No, the fan runs continuously during occupied and standby modes. If it is set to Yes, the fan cycles off when the temperature setpoints are satisfied.