NS sensor - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27

If the system has an NS sensor that has a warmer-cooler adjustment, a setpoint adjustment, or an onboard PIR occupancy sensor, you can perform the following actions:

  • Initiate a temporary occupancy state by adjusting the knob or pressing a button on the unit. You can adjust the amount of time that the unit remains in this temporary occupancy state by adjusting Temp Occupancy Time. To adjust the Temp Occupancy Time, navigate to the Commissioning > Setpoints menu. Set the time to zero to disable this feature.
  • Configure the amount of adjustability the occupants have with the warmer-cooler adjustment or Warm/Cool Adjust Range from the Commissioning > Setpoints menu. Set the range to 0 to disable this function.
  • On the Setpoints section of the Commissioning menu, configure the following parameters:
    • Deadband
    • Heat Cool Setpoint Mode
    • Individual Occupied Temperature Setpoint
    • Standby Setpoints
    • Common Occupied Temperature Setpoint
    • Unoccupied Setpoints
    • Temp Occupancy Time