Standby mode - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document number
LIT-12013067
Revision date
2023-04-27
Product status
Discontinued

Standby mode occurs when the schedule is set to occupied and the sensor is set to unoccupied. During standby mode, standby setpoints are active and the effective heating and cooling setpoints adjust accordingly. In the unoccupied mode, the unit remains off until the zone temperature rises above or falls below the unoccupied cooling or heating setpoints. When this occurs, the system reactivates to satisfy the zone temperature.