From the Status menu, use the built-in Unit Enable setting to manually shut down the unit. You can also use the global shutdown feature in Verasys to shut down the controller.
Note: To initiate the global shutdown command feature in Verasys, you must have a LC-VAC1002-0.
Note: You must have a LC-VAC1002-0 or a generic Input
Output Module (IOM) with a generic IOM application installed to initiate a
global shutdown command to Verasys. To initiate a global shutdown
command, ensure that BI-2 is a closed contact to the LC-IOM100-0 or LC-VAC1002-0.
For more information about configuring the generic IO application for global
shutdown, refer to the Global shutdown section of Verasys System
User Guide (LIT-12012371)
.